Hello NXP
Am with S32K148 with IDE S32 Design Studio. While am trying to debug with break points, cursor is not getting stopped at the break point. Observed threads got missed to track.
using on board debugger Open SDA
Please do the needfull.
Console Message:
Task name is Task_10ms
Task name is Task_2ms
Task name is Task_1ms
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F31306D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F316D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F326D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F356D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 5461736B5F3130306D73
rsp_qThreadExtraInfo - Thread extra info grabbed - result: 49444C45
Number of threads 9 qfThreadInfoIterator: 0
Number of threads 9 qfThreadInfoIterator: 9
 
					
				
		
 lukaszadrapa
		
			lukaszadrapa
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
it could be caused by optimizations. I would check if the optimization level is set to 0:
Regards,
Lukas
 
					
				
		
 lukaszadrapa
		
			lukaszadrapa
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi,
is OS Awareness enabled like this?
And if this doesn't help, is it possible to share the project, so we can try to reproduce the behavior on our side?
Thanks,
Lukas