Hi@Chandra13
1.Please make sure external 12V power supply was used for S32K148EVB,elsewise the CAN PTY will not work.
2. these two demo enabled the CAN FD features, so please make sure the PC software configuration is right.
3. I made a sample demo for your reference, you can try it, this demo should periodically send frames with ID 0x01(500K)

#include "sdk_project_config.h"
#include <stdint.h>
#include <stdbool.h>
volatile int exit_code = 0;
flexcan_msgbuff_t recvMsg;
flexcan_data_info_t dataInfo =
{
.data_length = 8U,
.msg_id_type = FLEXCAN_MSG_ID_STD,
.enable_brs = false,
.fd_enable = false,
.fd_padding = 0U
};
int main(void)
{
uint8_t DummyData[8] = {0};
/* Configure clocks for PORT */
CLOCK_DRV_Init(&clockMan1_InitConfig0);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
FLEXCAN_DRV_Init(INST_FLEXCAN_CONFIG_1, &flexcanState0, &flexcanInitConfig0);
/*Configure a Tx Message Buffer.*/
FLEXCAN_DRV_ConfigTxMb(INST_FLEXCAN_CONFIG_1, 0, &dataInfo, 0x01);
FLEXCAN_DRV_SetRxMaskType(INST_FLEXCAN_CONFIG_1,FLEXCAN_RX_MASK_GLOBAL);
FLEXCAN_DRV_SetRxMbGlobalMask(INST_FLEXCAN_CONFIG_1,FLEXCAN_MSG_ID_STD,0xFFFFFFFF);
/* Configure RX message buffer with index RX_MSG_ID and RX_MAILBOX */
FLEXCAN_DRV_ConfigRxMb(INST_FLEXCAN_CONFIG_1, 1, &dataInfo, 0x02);
/*Receives a CAN frame into a configured message buffer.*/
FLEXCAN_DRV_Receive(INST_FLEXCAN_CONFIG_1,1,&recvMsg);
while(1)
{
OSIF_TimeDelay(1000);
DummyData[0] = 0xff;
FLEXCAN_DRV_Send(INST_FLEXCAN_CONFIG_1,0,&dataInfo,0x01,DummyData);
}
for(;;) {
if(exit_code != 0) {
break;
}
}
return exit_code;
}