Maybe the mcu locked,but use JLink can not unlock,the Reset Pin is grounded.The program runs normally.
Hi wl z,
Please read the MDM_AP status and control registers by refer the steps descripted in Unbricking S32K146.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Thanks,but now i think the debug interface can not be used,because i can not find mcu through the J-Link Commander.
Before input "unlock kinetis", you should follow the tips of JLink Commander( Type "connect" to establish a target connection)
Sure,I tried again and again.
If it's your custom board, then please check the SWD connection by refer:AN5426: Hardware Design Guidelines for S32K1xx – Application Note
If you are using S32K148EVB, have you tried to debug it with onboard OpenSDA?
Thanks for your reply,it's my custom board,I use multimeter check the SWD connection and it's no problem.