S32K148 adc not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 adc not working

1,796 Views
guochuan
Contributor III

Our project uses S32K148 ADC0 and ADC1, and each ADC is configured with 8 channels. The test found that the last three channels could not obtain data.

guochuan_0-1681457159236.png

 

Tags (1)
0 Kudos
Reply
2 Replies

1,720 Views
Nhi_Nguyen
NXP Employee
NXP Employee

Hi guochuan,

I think the problem can come from this parameter is so small to convert data on all channels. So, you can try to adjust it.

Nhi_Nguyen_0-1682405950808.png

This is its description

Nhi_Nguyen_1-1682406052209.png

For example:

ADC's clock frequency is 40 MHz and prescaler value for frequency is 1.

Nhi_Nguyen_2-1682406118434.png

Nhi_Nguyen_6-1682406718717.png

 

PDB's clock frequency is 80MHz get from SYS_CLK

Follow to above expression for 1 ADC's channel: "ADC TOTAL CONVERSION TIME = Sample Phase Time (set by SMPLTS+1) + Hold Phase (1 ADC Cycle) + Compare Phase Time (8-bit Mode=20 ADC Cycles, 10-bit Mode=24 ADC Cycles,
12-bit Mode=28 ADC Cycles) + Single or First continuous time adder (5 ADC cycles + 5 bus clock cycles)."

SMPLTS: 

Nhi_Nguyen_3-1682406313533.png

I used 12 bit Mode.

In my case, ADC cycle = Bus cycle.

ADC TOTAL CONVERSION TIME = (255 + 1) + 1 + 28 + 10 = 295.

I have this parameter:

Nhi_Nguyen_4-1682406519940.pngNhi_Nguyen_5-1682406537209.png

So, I have: ADC TOTAL CONVERSION TIME  = 295 * 8 * 8 (channels) =  18880 (cycles)

This parameter Adc Delay Next PDB (0 -> 65535) have to ensure enough time to convert all pre-triggers in channel 0 and this value will be written as counter of PDB. So, we need to convert to PDB's cycles before write it into the register.

 (18880/ 40 * 80 = 37760)

Adc Delay Next PDB (0 -> 65535) have to configure bigger than 37760.

Best regards,

Nhi

 

 

0 Kudos
Reply

1,782 Views
guochuan
Contributor III

HI NXP team

Our project uses S32K148 ADC0 and ADC1, and each ADC is configured with 11 channels. The test found that the last three channels could not obtain data.

Tags (1)
0 Kudos
Reply