S32K148 - SJA1105 RMII connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 - SJA1105 RMII connection

Jump to solution
1,092 Views
matej_15
Contributor III

Hi!

We have an FS32K148UJT0VMHR SMCU and SJA1105QEL Ethernet Switch connected over RMII. Can you please confirm this connection is okay?

matej_15_0-1655817546868.png

 

Additionally, SMCU and PHYs connected to the Ethernet Switch all have MDC/MDIO interfaces. Ethernet Switch doesn't have it. Can we left MDC/MDIO interface on SMCU floating?

 

Best regards,

Matej

0 Kudos
1 Solution
1,072 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you can take a look at application note AH1604 which is available on docstore.nxp.com:

lukaszadrapa_0-1656001339260.png

MDC/MDIO (or called SMI) is used for configuration of PHYs. Here is an example from SJA1105SMBEVM board (MII or RMII between MCU and switch, SMI between MCU and PHYs):

lukaszadrapa_1-1656001468450.png

Regards

Lukas

 

View solution in original post

2 Replies
1,046 Views
matej_15
Contributor III

@lukaszadrapa thank you very much for the help!

0 Kudos
1,073 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you can take a look at application note AH1604 which is available on docstore.nxp.com:

lukaszadrapa_0-1656001339260.png

MDC/MDIO (or called SMI) is used for configuration of PHYs. Here is an example from SJA1105SMBEVM board (MII or RMII between MCU and switch, SMI between MCU and PHYs):

lukaszadrapa_1-1656001468450.png

Regards

Lukas