S32K148 IC CAN NOT BE DEBUGGED ON S32DS Platform3.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 IC CAN NOT BE DEBUGGED ON S32DS Platform3.4

121 Views
shaun_yue
Contributor I

Hi sir / miss

I have a problem about S32K148 IC can not be debugged on S32DS 3.4 .  The following is the problem phenomenon.

When I use S32DS to generate an adc project, just like "adc_hwtrigger_s32k148", then  configure debugging information . 

shaun_yue_0-1710328016468.png

shaun_yue_1-1710328033336.pngshaun_yue_2-1710328044157.png

And Rusume , it will go to STARTUP_S32K148.S , can not run normally and it also can not StepOver. 

shaun_yue_3-1710328282973.png

I tried other both examples "power_mode_switch_s32k148_mode" and "s32k148_test_erm", and both were OK. 

Please give me some reasonable advice .Thank you for your help .

 

 

 

0 Kudos
1 Reply

104 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @shaun_yue,

Could you confirm the version for the SDK you are using?  It is recommended to install S32K1 SDK RTM 4.0.3 with S32DS Extensions and Updates in S32DS v3.4.

Normally, this could be solved by performing a mass erase before flashing the MCU:

Julin_AragnM_0-1710369962181.png

Also, if you are using the evaluation board, please confirm you are following the documentation for the example: 

Julin_AragnM_1-1710370017120.png

Best regards,
Julián

0 Kudos