S32K148 Bootloader and RAppID BL Tool with Vector VN1640A

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K148 Bootloader and RAppID BL Tool with Vector VN1640A

2,447 次查看
markus_29
Contributor II

Hello all,

I am using the S32K1 EVAL BOARD with the S32K148.

I am trying to use the bootloader RAppID BL Tool to flash the application over CAN 0 (PTE4 and PTE5).

I am creating the application file using the Model-Based Design Toolbox (MBDT) in Simulink (C Coder).

I want to use a Vector CANCase (VN1640A) to flash the application.

Vector Hardware Config RAppID.png

 

RAppID BL Tool S32K1.png

Now I get this error.

Does anyone have any idea?

 

Thanks

Markus

0 项奖励
回复
4 回复数

2,433 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @markus_29 

Take a look at the community post: RAppID BL Tools for the S32K144. It is mentioned the same error that you are having.

 

B.R.

VaneB

0 项奖励
回复

2,411 次查看
markus_29
Contributor II

Hi VaneB

My problem is putting the board into Bootloader mode.

I hold the reset button (SW5) and then plug in the USB cable.

Set jumper J22 to 2-3 (Reset switch is routed to openSDA reset line).

I use the S32K148 EVAL BOARD.

 

Many greetings

 

0 项奖励
回复

2,274 次查看
mikedoidge
NXP Employee
NXP Employee

Hello Markus,

When you put the OpenSDA into Bootloader mode, this is to allow you to update the OpenSDA firmware. If you program this with the RAppID BL RBF file then it will get stuck in bootloader mode and you will be unable to use the board until you program a valid .SDA file from PEMicro and restore the OpenSDA firmware.

To program the RBF file, you just need to drag the file to the drive letter (while not set for Bootloader mode).

Best Regards,

Mike

0 项奖励
回复

2,397 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @markus_29 

If you are getting problems with the bootloader, let me suggest you take a look at the application note S32K1xx Bootloader.

0 项奖励
回复