S32K148 ADC Temp Sense

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K148 ADC Temp Sense

2,470 Views
m_mishrikey
Contributor III

I'm looking for information about the S32K148 temp sense feature.

In PEX component for ADC you can select input channel for temp sense: 

adc_temp_input.png

There is no information about this option in the S32K Reference Manual. 

This is the most relevant thread I could find on the topic however the answer is not public:

Does S32K provide temperature data? 

This thread indicates maybe it was removed as an option for the s32k144:

https://community.nxp.com/thread/458117 

What's the story?

Thanks,
Matt

0 Kudos
Reply
5 Replies

2,405 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Matthew Mishrikey,

Sorry for the inconvenience we bring you!
And thank you for your patience.

Here is the feedback from internal team: We are working to add in the new revision of the RM the information about the internal temp sensor.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,365 Views
paulsiegel
Contributor I

When will this RM be available?

thanks Paul

0 Kudos
Reply

2,404 Views
m_mishrikey
Contributor III

That's good news.  In lieu of the updated RM, may I please have a demo program that can do the internal temp sensor read?

0 Kudos
Reply

2,341 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

There is no demo program at the moment. And I don't have the date of the released of the new RM.
If you have NDA signed, I can share the preliminar documents to you through Support Tickets.

0 Kudos
Reply

1,913 Views
florian_bayer
Contributor II

@Robin_Shen could you please send me information about that too ? 

0 Kudos
Reply