S32K146 of SPI send by SDK failed 😥

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 of SPI send by SDK failed 😥

1,691 Views
mrsong
Contributor II

i used spi through SDK to send data but failed if the txbuffer was set large(such as 600 bytes) and rxbuffer was set NULL.  and if the txbuffer was set smaller(such as 2 bytes) ans rxbuffer was set NULL ,it's valid . here's how i tired to send it

    . failed (Txbuffer set 600 bytes ,and rxbuffer set NULL)

 pastedImage_2.png

    . successed (Txbuffer set 2 bytes ,and rxbuffer set NULL)

pastedImage_3.png

    . successed (Txbuffer set 600 bytes ,and rxbuffer set 600 Bytes)

pastedImage_4.png

i saw the SDK said "receiveBuffer Pointer to the buffer where the received bytes are stored. If you pass NULL
* for this parameter, the received bytes are ignored" and i don't need the rxbuffer either ,if i use step3 (③) to send ,this will take up a lot of memory .

pastedImage_5.png

hope to resolve this question soon . 

Best wishes .

Labels (1)
3 Replies

1,539 Views
nxf25521
NXP Employee
NXP Employee

Hi Mr Song ,
- Could you please provide me more detail about SDK release version which you used ?

0 Kudos
Reply

1,539 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello,

Thank you for the report.

This issue is investigated by the SDK team.

If I receive more details from them I will inform you.

Best regards,

Diana

0 Kudos
Reply

1,539 Views
347996379
Contributor III

Hi,Diana

Has the problem been solved?What causes it?

0 Kudos
Reply