S32K146 SW and HW details

cancel
Showing results for 
Search instead for 
Did you mean: 

S32K146 SW and HW details

1,173 Views
ravirajns
Contributor II

Hi,

We are planning to use S32K146 (FS32K146HFT0VMHR) for our project where LIN, CAN, UART, SPI etc peripherals going to connect.

Below are some queries :

1. What are tested drivers available for S32K and what is maturity?

2. Is any default OS available?

3. Any OS ported on S32K and tested ?

4. Any certification done ?

5. Is there any evaluation board available for S32K146 or S32K144 evaluation board can be used?

6. What are HW and SW tools are available.

7. We need to buy evaluation board, from where we can buy.

Please provide inputs on above points.

Thanks,

Raviaj

0 Kudos
1 Reply

476 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

There is a quality package available only for SDK 1.0.0 RTM which includes FreeRTOS driver but it supports S32K144 only, see Release notes. Evaluation boards for S32K146 are not available yet. However, there should be prototypes, please contact your distributor.

 

Regards,

Daniel

0 Kudos