Hello the community,
I am working on NXP S32K146 µc and S32DS IDE.
I have an issue on SPI with chip select management. The µc is configured in master, and it communicates with 2 slaves on CS0 and CS3.
Firstly, the µc communicate on CS0 --> OK
Secondly, the µc communicate on CS3 --> OK
But if :
Firstly, the µc communicate on CS3 --> OK
Secondly, the µc communicate on CS0 --> NOK
I check the register TCR (bits PCS) when I active both CSx and everything is ok. But when I have checked on scope, I saw, as soon as CS3 is selected, the pin CS3 stays activated and never CS0.
My question is, what I have to do when I want to change the CS, the register TCR (PCS) is not enought ? (Of course the CS is not changed during transfert)
Thanks by advance
Sebastien
Hello Daniel,
thanks for your answers I did not see the TCR register is usable only in stop mode.
So what is the process (the code source) to change chip select ?
Because I am a little lost.
Regards
Sebastien
Hi Sebastien,
I recommend the following procedure:
LPSPI0->TCR = LPSPI_TCR_CPHA_MASK | LPSPI_TCR_CPOL_MASK | LPSPI_TCR_PRESCALE(1) | LPSPI_TCR_FRAMESZ(15);
//Send data with PCS 0;
LPSPI0->TCR = LPSPI_TCR_CPHA_MASK | LPSPI_TCR_CPOL_MASK | LPSPI_TCR_PRESCALE(1) | LPSPI_TCR_FRAMESZ(15) | LPSPI_TCR_PCS(3);
//Send data with PCS 3;
LPSPI0->TCR = LPSPI_TCR_CPHA_MASK | LPSPI_TCR_CPOL_MASK | LPSPI_TCR_PRESCALE(1) | LPSPI_TCR_FRAMESZ(15);
//Send data with PCS 0;
The main point is to use only one write operation to handle TCR. If you do something like this: clear PCS and then set PCS in TCF fifo are 2 elements and first frame sent will use PCS0 (configured by clear operation) and the second frame will use the PCS configured by your application.
Best regards,
Razvan
Hi Sebastien,
The TCR register is not an ordinary register, it is a FIFO.
The read-modify-write operations that you are doing are not good in this case.
Section 49.3.1.15.2 S32K1xx RM rev.8 discusses problems of reading the register.
You can prepare the commands in variables/constants a then simply write them in the TCR register.
LPSPI0->TCR = command;
Regards,
Daniel
Hello,
I answer myself, because I find a solution :
Before I had:
/* Remove actual chip select */
LPSPI0->TCR &= ~LPSPI_TCR_PCS_MASK;
/* Write new chip select */
LPSPI0->TCR |= LPSPI_TCR_PCS(u8ChipSelected);
Now I have:
LPSPI0->TCR = LPSPI_TCR_CPHA_MASK
| LPSPI_TCR_CPOL_MASK
| LPSPI_TCR_PRESCALE(1)
| LPSPI_TCR_FRAMESZ(15);
LPSPI0->CR |= LPSPI_CR_MEN_MASK;
/* Remove actual chip select */
LPSPI0->TCR &= ~LPSPI_TCR_PCS_MASK;
/* Write new chip select */
LPSPI0->TCR |= LPSPI_TCR_PCS(u8ChipSelected);
Best regards
Sebastien