S32K146 MCU which pins support external interrupt function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 MCU which pins support external interrupt function

325 Views
Cynthia
Contributor I

The first question is: which pins of S32K146 microcontroller support external interrupt function. The second question is: are there clamp diodes on the internal pins of S32K146 microcontroller, and if so, which pins are there?

0 Kudos
1 Reply

321 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Cynthia 

The PORT pins support external interrupt and have always ESD clamping diodes.

Note: refer 'IO Signal Table' tab of IO Signal Description Input Multiplexing sheet attached to the Reference Manual.

 

B.R.

VaneB

0 Kudos