S32K146 GPIO PAD resistance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 GPIO PAD resistance

Jump to solution
1,076 Views
lihui1
Contributor II

 For there is require on GPIO input current , we want to know what is the resistance in this red box

CatchC2E5(07-21-(07-21-19-35-22).jpg

0 Kudos
Reply
1 Solution
1,060 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
5 Replies
1,065 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@lihui1

you can find this information in S32K-DS.pdf : S32K1xx Data Sheet Rev.14,08/2021

5.3 DC electrical specifications at 3.3 V Range.

Senlent_0-1658455562809.png

5.4 DC electrical specifications at 5.0 V Range.

Senlent_1-1658455680184.png

 

0 Kudos
Reply
1,063 Views
lihui1
Contributor II

So it's not current-limiting resister ? It's pullup/pulldown resistor? 

Tags (1)
0 Kudos
Reply
1,061 Views
Senlent
NXP TechSupport
NXP TechSupport

yes

0 Kudos
Reply
1,055 Views
lihui1
Contributor II

and a liitle more question we want to know:

If GPIO used as input,  has this resister there on the input circuit?

It seems like input current will flow through this resistor as below

37f25c5c6e00de5e1507209b8fb96dc.jpg

0 Kudos
Reply
1,058 Views
lihui1
Contributor II

OK!  Thank you!

0 Kudos
Reply