S32K146 FlexRam Regional data is abnormal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K146 FlexRam Regional data is abnormal

Jump to solution
1,265 Views
Louis1916
Contributor III

The customer's engineer feedback received 2pcs fault board from the market side,After preliminary analysis, it is believed that the data in the FlexRam region is abnormal.

1.Engineers want to know what could cause damage to the FlexRam area? Why Can a Read Operation Be Executed Smoothly but a Write Operation Is Abnormal?

2.Why does a write operation to a FlexRam zone affect the data in a FlexNVM zone?

Thanks!

Tags (1)
0 Kudos
Reply
1 Solution
1,242 Views
Senlent
NXP TechSupport
NXP TechSupport

 

Hi@Louis1916

Sorry for the later reply.

From the perspective of the EEPROMDE mechanism, reading the internal EEPROM will not access the FlexNVM area, but directly access the FlexRam area.

The write operation is different. When you write FlexRam, it needs to synchronize the FlexRam value to FlexNVM for backup. We need to wait for the backup to complete before writing the new value, otherwise it may cause hardfault.

The above are the differences between the two operations

 

Regarding the RDCOLERR error, you can refer to the following section of the application note AN11983

 

Senlent_1-1736406941652.png

 

View solution in original post

0 Kudos
Reply
1 Reply
1,243 Views
Senlent
NXP TechSupport
NXP TechSupport

 

Hi@Louis1916

Sorry for the later reply.

From the perspective of the EEPROMDE mechanism, reading the internal EEPROM will not access the FlexNVM area, but directly access the FlexRam area.

The write operation is different. When you write FlexRam, it needs to synchronize the FlexRam value to FlexNVM for backup. We need to wait for the backup to complete before writing the new value, otherwise it may cause hardfault.

The above are the differences between the two operations

 

Regarding the RDCOLERR error, you can refer to the following section of the application note AN11983

 

Senlent_1-1736406941652.png

 

0 Kudos
Reply