S32K146-EVB demo debug fail (connect fialed)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K146-EVB demo debug fail (connect fialed)

2,122 次查看
mrsong
Contributor II

hi ,i met a problem about S32K146 demo board connect failed .

i tried to set  "emergency kinetis device recovery by full chip erase"  but cant launch failed either , and i tested the voltage about reset pin is 3.3V or 5V to make sure the power was ok . PE was failed to conncet either .

so do you have any other ways to fix this problem?

The attachment were the question i met

B&R

Aaron

标记 (1)
0 项奖励
回复
1 回复

2,041 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Mr Song

Were you able to program the board before? what was the last program that you used? Also, have you modified the jumpers settings of the board? I recommend you to check this in the link:

Get Started with the S32K146EVB | NXP 

You can also try to update the openSDA to the last version of the P&EMicro firmware, you can download it from their web page.

Hope this helps

Best regards

0 项奖励
回复