Q1: CAN-FD data phase only set max 1000kbit/s ?
Q2 : CAN-FD:
if the CAN bus is connected when the machine is started, the transceiver is normal;
but cannot send out data return BUSY while hot-plug.
if (state->mbs[mb_idx].state != FLEXCAN_MB_IDLE)
{ return STATUS_BUSY; }
Hi,
1) theoretically up to 8Mbps is supported, but this is also limited by used PE clock, transceiver and real bus.
2) there should not be problem with hot-plug. If the MB cannot still be used for transmission, try to first AbortTransfer and then send message normally.
BR, Petr
hello,
set Data phase to MAX 1600kbit/s by ProcessorExpert.pe
Hi,
use crystal with higher frequency or select system clock as PE clock source.
BR, Petr