S32K144EVB-Q100 Shield footprint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144EVB-Q100 Shield footprint

613 Views
jzhang1
Contributor II

Hi,

I want to make a prototype board attached to the S32K144EVB-Q100.

Does anyone have the footprint for the layout of S32K144EVB-Q100? 

I only need to know the board dimension with its J-header pin layout.

Thanks.

0 Kudos
3 Replies

601 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@jzhang1

I sent you the hardware design package privately,please check the attachments.

BR!

     Jim,

574 Views
jzhang1
Contributor II

Hi @Senlent , thanks for sending the schematic. 

By the way, does the VDD on board (ex. J5-10, J6-10) configurable (On and Off)? Or does VDD mean to continuously provide 5V or 3.3V  as long as the board is powered?

 

Thanks.

0 Kudos

561 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@jzhnag1

J5-10 can be connected to VDD, which means you can connect ports that need power to J5-10.

If J107 is not connected, the S32K144EVB should cut off all power unless you choose a power supply.

Senlent_0-1649209035199.png

BR!

      Jim,

 

0 Kudos