Hi,
I want to make a prototype board attached to the S32K144EVB-Q100.
Does anyone have the footprint for the layout of S32K144EVB-Q100?
I only need to know the board dimension with its J-header pin layout.
Thanks.
Hi @Senlent , thanks for sending the schematic.
By the way, does the VDD on board (ex. J5-10, J6-10) configurable (On and Off)? Or does VDD mean to continuously provide 5V or 3.3V as long as the board is powered?
Thanks.
J5-10 can be connected to VDD, which means you can connect ports that need power to J5-10.
If J107 is not connected, the S32K144EVB should cut off all power unless you choose a power supply.
BR!
Jim,