S32K144 with LCD 1602A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 with LCD 1602A

331 Views
gksn284
Contributor I

Hello.

I want to use LCD in S32K144. (LCD 1602A or LCD 1602A + I2C)

Is there no related library or code?

Please help me.

0 Kudos
1 Reply

320 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi gksn284,

I didn't find any ready code for s32k144 to implement LCD 1602A. However, you can refer to the following post using Kinetis MCU: Driving 16x2 LCD using KSDK drivers


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos