S32K144 is stuck

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 is stuck

Jump to solution
851 Views
kmh48301
Contributor IV

Hi

 

I inserted csec key and I Erased first sector in Pflash (0x0 address)

 

so, when i plug in debugger, it tries to mass erase. but because it has csec key, mass erase doesn't work.

 

I need to use this s32k144-evb-q100.... 

 

Please help me.

 

Thanks

Best Regards

Phillip

0 Kudos
Reply
1 Solution
838 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Phillip,

in short - there's no way to recover.

If the flash configuration field is erased, FSEC is 0xFF and the device is secured. To unsecure the device, it's necessary to perform mass erase. But if CSE is enabled, mass erase cannot be exeucted. It would be necessary to destroy the partition using CMD_DBG_CHAL and CMD_DBG_AUTH when you need to also know MASTER_ECU_KEY. There's no way to escape this circle.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
1 Reply
839 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Phillip,

in short - there's no way to recover.

If the flash configuration field is erased, FSEC is 0xFF and the device is secured. To unsecure the device, it's necessary to perform mass erase. But if CSE is enabled, mass erase cannot be exeucted. It would be necessary to destroy the partition using CMD_DBG_CHAL and CMD_DBG_AUTH when you need to also know MASTER_ECU_KEY. There's no way to escape this circle.

Regards,

Lukas

0 Kudos
Reply