S32K144 firmware update via CAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K144 firmware update via CAN

3,449 次查看
thanhchu_ict
Contributor II

标记 (1)
8 回复数

3,088 次查看
siddharth_sameer
Contributor II

Hey @dianabatrlova @thanhchu_ict 

I was looking for the demo code for S32K144 use case in AN12323. It would be a great help if you guys attach them in reply to this post.

Thanks in advance

Siddharth Sameer

 

0 项奖励
回复

3,287 次查看
thanhchu_ict
Contributor II

Hi all, i have followed example in https://www.nxp.com/docs/en/application-note/AN12323.pdf  to update firmware for S32K144 via CAN but when i implement that example,i stuck in some troubles. I created some other binary file (blink LED using clock...) like two binary file in the document but it didn't work, although i tried to implement code PIC option(in S32DS), code ROPI/RWPI (in IAR IDE), modified linker files... Do you have any ideals or solutions to deal with that problem? 

0 项奖励
回复

3,287 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

At first, I would like to know, have you tried default already existing binary files?

Does it work?

If yes, a linker file of your own project may not be well configured.

How did you recognize that it didn't work, any error during loading the .bin file, or after the jump into the application?

Best regards,

Diana

3,287 次查看
thanhchu_ict
Contributor II

hi,

i had tried the default binary files in the example and it completely work, but when i created another by myself, it can't jump to the address of the application, I used helloworld_clock example in the NXP's library to generated binary file, but it didn't blink anymore. Could you please tell me how can i deal with the linker file?

Sincerely,

ThanhChu.

0 项奖励
回复

3,287 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi, 

Can you, please, share your linker file?  It is located in the project folder in "Project_Settings\Linker_Files". 

I would like to check it.

Thank you.

Best regards,

Diana

0 项奖励
回复

3,287 次查看
thanhchu_ict
Contributor II

Hi, 

Here it is.

Sincerely.

----------------------------------------

ENTRY(Reset_Handler)

/*
To use "new" operator with EWL in C++ project the following symbol shall be defined
*/
/*EXTERN(_ZN10__cxxabiv119__terminate_handlerE)*/

HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0x00000400;
STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00000400;

/* If symbol __flash_vector_table__=1 is defined at link time
* the interrupt vector will not be copied to RAM.
* Warning: Using the interrupt vector from Flash will not allow
* INT_SYS_InstallHandler because the section is Read Only.
*/
M_VECTOR_RAM_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : 0x0400;

/* Specify the memory areas */
MEMORY
{
/* Flash */
m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0

/* SRAM_L */
m_data (RW) : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000

/* SRAM_U */
m_data_2 (RW) : ORIGIN = 0x20000000, LENGTH = 0x00007000
}

/* Define output sections */
SECTIONS
{
/* The startup code goes first into internal flash */
.interrupts :
{
__VECTOR_TABLE = .;
. = ALIGN(4);
KEEP(*(.isr_vector)) /* Startup code */
. = ALIGN(4);
} > m_interrupts

.flash_config :
{
. = ALIGN(4);
KEEP(*(.FlashConfig)) /* Flash Configuration Field (FCF) */
. = ALIGN(4);
} > m_flash_config

/* The program code and other data goes into internal flash */
.text :
{
. = ALIGN(4);
*(.text) /* .text sections (code) */
*(.text*) /* .text* sections (code) */
*(.rodata) /* .rodata sections (constants, strings, etc.) */
*(.rodata*) /* .rodata* sections (constants, strings, etc.) */
*(.glue_7) /* glue arm to thumb code */
*(.glue_7t) /* glue thumb to arm code */
*(.eh_frame)
KEEP (*(.init))
KEEP (*(.fini))
. = ALIGN(4);
} > m_text

.ARM.extab :
{
*(.ARM.extab* .gnu.linkonce.armextab.*)
} > m_text

.ARM :
{
__exidx_start = .;
*(.ARM.exidx*)
__exidx_end = .;
} > m_text

.ctors :
{
__CTOR_LIST__ = .;
/* gcc uses crtbegin.o to find the start of
the constructors, so we make sure it is
first. Because this is a wildcard, it
doesn't matter if the user does not
actually link against crtbegin.o; the
linker won't look for a file to match a
wildcard. The wildcard also means that it
doesn't matter which directory crtbegin.o
is in. */
KEEP (*crtbegin.o(.ctors))
KEEP (*crtbegin?.o(.ctors))
/* We don't want to include the .ctor section from
from the crtend.o file until after the sorted ctors.
The .ctor section from the crtend file contains the
end of ctors marker and it must be last */
KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors))
KEEP (*(SORT(.ctors.*)))
KEEP (*(.ctors))
__CTOR_END__ = .;
} > m_text

.dtors :
{
__DTOR_LIST__ = .;
KEEP (*crtbegin.o(.dtors))
KEEP (*crtbegin?.o(.dtors))
KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors))
KEEP (*(SORT(.dtors.*)))
KEEP (*(.dtors))
__DTOR_END__ = .;
} > m_text

.preinit_array :
{
PROVIDE_HIDDEN (__preinit_array_start = .);
KEEP (*(.preinit_array*))
PROVIDE_HIDDEN (__preinit_array_end = .);
} > m_text

.init_array :
{
PROVIDE_HIDDEN (__init_array_start = .);
KEEP (*(SORT(.init_array.*)))
KEEP (*(.init_array*))
PROVIDE_HIDDEN (__init_array_end = .);
} > m_text

.fini_array :
{
PROVIDE_HIDDEN (__fini_array_start = .);
KEEP (*(SORT(.fini_array.*)))
KEEP (*(.fini_array*))
PROVIDE_HIDDEN (__fini_array_end = .);
} > m_text

__etext = .; /* Define a global symbol at end of code. */
__DATA_ROM = .; /* Symbol is used by startup for data initialization. */
.interrupts_ram :
{
. = ALIGN(4);
__VECTOR_RAM__ = .;
__interrupts_ram_start__ = .; /* Create a global symbol at data start. */
*(.m_interrupts_ram) /* This is a user defined section. */
. += M_VECTOR_RAM_SIZE;
. = ALIGN(4);
__interrupts_ram_end__ = .; /* Define a global symbol at data end. */
} > m_data

__VECTOR_RAM = DEFINED(__flash_vector_table__) ? ORIGIN(m_interrupts) : __VECTOR_RAM__ ;
__RAM_VECTOR_TABLE_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : (__interrupts_ram_end__ - __interrupts_ram_start__) ;

.data : AT(__DATA_ROM)
{
. = ALIGN(4);
__DATA_RAM = .;
__data_start__ = .; /* Create a global symbol at data start. */
*(.data) /* .data sections */
*(.data*) /* .data* sections */
KEEP(*(.jcr*))
. = ALIGN(4);
__data_end__ = .; /* Define a global symbol at data end. */
} > m_data

__DATA_END = __DATA_ROM + (__data_end__ - __data_start__);
__CODE_ROM = __DATA_END; /* Symbol is used by code initialization. */
.code : AT(__CODE_ROM)
{
. = ALIGN(4);
__CODE_RAM = .;
__code_start__ = .; /* Create a global symbol at code start. */
*(.code_ram) /* Custom section for storing code in RAM */
. = ALIGN(4);
__code_end__ = .; /* Define a global symbol at code end. */
} > m_data

__CODE_END = __CODE_ROM + (__code_end__ - __code_start__);

/* Custom Section Block that can be used to place data at absolute address. */
/* Use __attribute__((section (".customSection"))) to place data here. */
.customSectionBlock ORIGIN(m_data_2) :
{
KEEP(*(.customSection)) /* Keep section even if not referenced. */
} > m_data_2

/* Uninitialized data section. */
.bss :
{
/* This is used by the startup in order to initialize the .bss section. */
. = ALIGN(4);
__BSS_START = .;
__bss_start__ = .;
*(.bss)
*(.bss*)
*(COMMON)
. = ALIGN(4);
__bss_end__ = .;
__BSS_END = .;
} > m_data_2

.heap :
{
. = ALIGN(8);
__end__ = .;
PROVIDE(end = .);
PROVIDE(_end = .);
PROVIDE(__end = .);
__HeapBase = .;
. += HEAP_SIZE;
__HeapLimit = .;
__heap_limit = .;
} > m_data_2

.stack :
{
. = ALIGN(8);
. += STACK_SIZE;
} > m_data_2

/* Initializes stack on the end of block */
__StackTop = ORIGIN(m_data_2) + LENGTH(m_data_2);
__StackLimit = __StackTop - STACK_SIZE;
PROVIDE(__stack = __StackTop);

.ARM.attributes 0 : { *(.ARM.attributes) }

ASSERT(__StackLimit >= __HeapLimit, "region m_data_2 overflowed with stack and heap")
}

0 项奖励
回复

3,287 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Thank you for sharing the linker file, I can see that you didn't change anything. 

Firmware is located in a certain place in the memory, that is why to change the Linker File is needed.

Please, refer to the AN12323:

https://www.nxp.com/docs/en/application-note/AN12323.pdf 

"Finally, when developing the bootloader firmware, the location in memory should be considered. Bootloader firmware and application might reside in the same NVM memory block, hence it is necessary to modify bootloader and application firmware linker files to avoid overlaps. There are some devices that have a dedicated location in memory to place the bootloader. Linker file modification depends on the microcontroller and compiler that is used."

In the AN12323, you can see the "Figure 12 - S32K144 update process" there is a structure of the memory space.

Could you try to use these linker file settings?

S32K144 firmware update AN12323 

Thank you.

Best regards,

Diana

0 项奖励
回复

3,287 次查看
thanhchu_ict
Contributor II

Thank you so much!

0 项奖励
回复