S32K144 Watchdog accruacy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 Watchdog accruacy

275件の閲覧回数
Hoon
Contributor I

Hi.
I'm designing Watchdog using S32K144 and my settings are as follows
My intentions are as follows
2048(Timeout Value) / (128kHz(LPO) / 256(Prescaler)) = 4.096s
But, The actual Watchdog occurs approximately 4.7s later. (Test will be conducted after Watchdog count clear).
Even considering Accuracy of LPO, there is a big difference between 4.096s and 4.7s, is there any way to improve this?


[Watchdog setting]

Read only : Yes
Prescaler Enable : Yes
Update Enable : Yes
Interrupt Enable : Yes
Window Enable : No
Window Value : 0       [clock cycles]
Timeout Value : 2048 [clock cycles]
Wait Mode : No
Stop Mode : No
Debut Mode : No

0 件の賞賛
返信
1 返信

251件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I changed the configuration of wdog_interrupt_s32k144_SDK403 based on your tips.  

That project will feed the dog 8 times in the WDOG interrupt, and each time it feeds the dog, it will flip PTD15. After that, it will no longer feed the dog and wait for the watchdog reset.
I measured the time from the last time the dog was fed(flip the PTD15) to the next reset was about 4s.

wdog_interrupt_s32k144_SDK403 Reset_b PTD15.png

My test result is different from yours, I recommend testing the SDK example.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信