S32K144 VREFH what are the effects of different options?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 VREFH what are the effects of different options?

1,007 Views
jingfang
Contributor IV

VREFH has the following three options,what's the difference between these three terms?

Whether the function safety level B ia affected?

捕获(11).JPG

0 Kudos
Reply
2 Replies

991 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @jingfang,

These are just a few options that the EVB allows.

1. VDD_MCU is connected to VDDA. Therefore, VREF = VDDA.

2. If VDD_MCU is 5V, VREFH can be 3V.

3. You can use whatever voltage reference connected to AREF.

This specification must be met:

danielmartynek_0-1652696324074.png

Regarding function safety, please refer to the S32K1xx Safety Reference Manual that is available in SafeAssure NDA community group:

https://community.nxp.com/groups/safeassure-nda

I you don't have access, please follow this document:

https://community.nxp.com/docs/DOC-335524

 

Regards,

Daniel

 

 

 

0 Kudos
Reply

984 Views
jingfang
Contributor IV

Thanks a lot~

I have S32K1xx Series Safety Manual , is it ok?

0 Kudos
Reply