Hello EveryOne,
I developed on S32K144 board by SDK, I want to send data and receive data by uart, now I find MCU can receive the data through uart port, and I want to check the receiving status through the interface "LPUART_DRV_GetReceiveStatus", the return status is always STATUS_BUSY.
Hi
Where did LPUART_DRV_GetReceiveStatus return STATUS_BUSY?
Did you mean the LPUART_DRV_GetReceiveStatus in UART_EVENT_RX_FULL event?
Or call LPUART_DRV_GetReceiveStatus in uart_rx_end_check_task?
I'm not sure what uart_rx_end_check_task is trying to achieve, maybe it's possible to add other event like UART_EVENT_END_TRANSFER or UART_EVENT_ERROR in lpuart0_RX_ISR.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Robin_Shen,
Add question:
How can I make sure the datas arereceived end through UART?
when the LPUART_DRV_GetReceiveStatus() function returns value is STATUS_SUCCESS? now the return value keep STATUS_BUSY.
I meet the same issue,do you solve it ? can you get the currect status?
Hello Robin_Shen,
Sorry, I not descript the peoblem clearly.
The problem is as below information:
1. MCU can entry the RX IRQ normally.
2. MCU receive the data OK.
My question:
The system cannot enter the marked code block, LPUART_DRV_GetReceiveStatus() return value keeps STATUS_BUSY, I can not to check whther the datas received end.
Have you tried to add: else if(event == UART_EVENT_END_TRANSFER) {} in lpuart0_RX_ISR? When there is no more date need to be received(you don't call LPUART_DRV_SetRxBuffer anymore), it will enter this event.