[S32K144] RTD missing LinIf.xdm, Tresos can't create module LinIf

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32K144] RTD missing LinIf.xdm, Tresos can't create module LinIf

Jump to solution
333 Views
nbgddddd
Contributor I

Hello,

 

I have a question regarding the usage of LinIf plugin from the RTD in Tresos.

When trying to add LinIf module in Tresos it returns the following error:

nbgddddd_0-1743507161812.png

Module "LinIf_TS_T40D2M30I0R0" (defined in plugin "LinIf_TS_T40D2M30I0R0") defines the schema file "config/LinIf.xdm" which cannot be found (if the file is signed or crypted, it must be referenced in META-INF\CRYPTOMANIFEST.MF).

 

Unlike other modules, LinIf folder does not have a config folder where LinIf.xdm should have been

nbgddddd_1-1743507282665.png

Is ths a wrong installation or should the LinIf.xdm be generated separately somehow?

There is no LinIf.xdm in older RTD installations either.

 

Thanks!

 

 

0 Kudos
Reply
1 Solution
316 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @nbgddddd,

Please refer to the release notes for the RTD release (Version 3.0.0). You can see in the "Support and Delivered drivers" section, the LinIf driver delivered with the RTD is only a stub, it does not support configuration.

Julin_AragnM_0-1743528691712.png

This is only for testing purpose from our side. You should use CanIf, EthIf & LinIf from a third-party provider, such as Elektrobit (EB), Vector, etc. 

Best Regards,
Julián

View solution in original post

1 Reply
317 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @nbgddddd,

Please refer to the release notes for the RTD release (Version 3.0.0). You can see in the "Support and Delivered drivers" section, the LinIf driver delivered with the RTD is only a stub, it does not support configuration.

Julin_AragnM_0-1743528691712.png

This is only for testing purpose from our side. You should use CanIf, EthIf & LinIf from a third-party provider, such as Elektrobit (EB), Vector, etc. 

Best Regards,
Julián