S32K144 MPU Flash violate

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 MPU Flash violate

357件の閲覧回数
Junkie
Contributor I

Hi community members,

I configure RGD1 to protect Flash memory from core read and write(use FTFC).

Following is the profile i have initialized MPU with.

{

MPU->RGDAAC[0] = MPU_RGDAAC_M1UM(0x7) | MPU_RGDAAC_M1SM(0x3) | MPU_RGDACC_M0SM(0x3);

MPU->RGD[1].WORD0 = 0x77000;

MPU->RGD[1].WORD1 = 0x7801F;

MPU->RGD[1].WORD2 = MPU_RGD_WORD2_M1UM(0x7) | MPU_RGDAAC_M1SM(0x3) | MPU_RGD_WORD2_M0UM(0x0) | MPU_RGD_WORD2_M0SM(0x3);

MPU->RGD[1].WORD3 = MPU_RGD_WORD3_VLD(1);

}

(1) - then read:

tmp = *((uint32_t *)0x77000);

(2) - and then use FTFC command erase 0x77000 and write to 0x77000

 

BusFault will happen after (1), but MPU->CESR[SPERR2] been set not MPU->CESR[SPERR0].

No Busfault( or HardFault) will occur after (2).(I use debugger watch the address, it has been changed.)

0 件の賞賛
1 返信

340件の閲覧回数
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Junkie,

Regarding the first question, the description is not complete, please share the project or at least complete MPU initialization code.

The MCU can't prevent programming the flash, because the core does not write the flash directly, it programs the flash using the FTFC controller.

 

Regards,

Daniel

 

 

 

0 件の賞賛