S32K144: FlexRAM as Emulated EEPROM Initial Values?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K144: FlexRAM as Emulated EEPROM Initial Values?

跳至解决方案
2,877 次查看
mahmoudsherrah
Contributor III

I succeeded in configuring FlexRAM as emulated EEPROM and it is working as expected. I only wanted to know how to set initial values in this EEPROM.

I tried to do the following (struct initialization):

typedef struct

{
      uint8_t u8;

      uin16_t u16;
} eeerom_data_t;

__attribute__ ((section(".eeeprom"))) eeerom_data_t eeerom_data = {.u8 = 12, .u16 = 3456};

But unfortunately didn't work, I think because the FlexRAM area is set to 1's on flashing the software to S32K144.

Is there any way to achieve initial values of FlexRAM as emulated EEPROM? Thanks

标签 (1)
1 解答
2,074 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
The system should not access the data in FlexRAM until the flash controller completes the initialization indicated by the FCNFG[EEERDY] flag.
If you need to have the EEPROM initialized, copy the data from Flash once the EEPROM is ready.

Regards,
Daniel

在原帖中查看解决方案

4 回复数
2,075 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,
The system should not access the data in FlexRAM until the flash controller completes the initialization indicated by the FCNFG[EEERDY] flag.
If you need to have the EEPROM initialized, copy the data from Flash once the EEPROM is ready.

Regards,
Daniel

2,074 次查看
mahmoudsherrah
Contributor III

Unfortunately, this wastes program memory but I assume it's not that big of an issue. I also think this is the only way to do it. Thanks anyway.

0 项奖励
回复
2,074 次查看
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

In AN12130, there is:

pastedImage_1.png

If your programmer/debugger supports scripting, you can use a script to check the EEERDY flag and to write the data.
But this is not a question on the MCU but rather on the programmer.

Regards,
Daniel

0 项奖励
回复
2,074 次查看
mahmoudsherrah
Contributor III

Thanks for the link. It's interesting but as you said it is programmer work not SW. I think copying from flash to FlexRAM after EEERDY does the trick.

0 项奖励
回复