[S32K144] FlexIO - config two groups of uart

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32K144] FlexIO - config two groups of uart

1,127 Views
呈源黄
Contributor I

Hi, can I config two groups of UART by FlexIO?

Tags (1)
0 Kudos
Reply
2 Replies

989 Views
dianabatrlova
NXP TechSupport
NXP TechSupport

Hi,

Yes, you can configure 2x UART by FlexIO.

Note:

If we check chapter "52.1.1 FlexIO Configuration" in the RM rev 9. we can see that there are 4x Timer, 4x Shifter, and 8x Pin.

For the one UART receive we need 1x shifter and 1x timer and for the transmit, we need 1x shifter and 1x timer.

So, we can configure max 2x UART by FlexIO.

I hope it helps.

Best Regards,

Diana

0 Kudos
Reply

933 Views
Simin
Contributor II

Hi,

        If I want using FLEXIO shifter working in ‘Match store mode’ or 'Match continuous mode'

        Could you help me how to configure this function,and the applicaton case when we use

these two mode

Best regard,

Simin

0 Kudos
Reply