S32K144 + FS2303 SBC reset not released

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 + FS2303 SBC reset not released

1,514 Views
ThijsK
Contributor III

Hi,

I have an issue with the reset line repetitivly being asserted between a S32K144 MCU and a FS2303 SBC.

In my design RSTB of the SBC is connected to PTA5 of the MCU with the recommended RC pull-up from the SBC datasheet:

ThijsKesselsARRK_0-1744971482998.png

(VDDIO = SBC V1 = 5V)

When reset reaches 3V, it gets pulled low to 0V and released after 120µs, in a repeating pattern:

ThijsKesselsARRK_1-1744971838943.bmp

Supply voltages all seem happy: 5V, 3.3V, 1.6V on SBC and 5V on the MCU.

Am I overlooking something, or what could be going on here?

Kind regards,

Thijs

#FS32K144ULT0VLHT #MFS2303BMBA3EP

 

 

Tags (3)
0 Kudos
Reply
6 Replies

1,459 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Thijs,

If it is a blank chip that has not been programmed, please download the program after unsecure MCU by mass erase.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,419 Views
ThijsK
Contributor III

You mean the MCU? The J-Link cannot connect because reset is not released (kept low). The SBC should be pre-configured by NXP:

ThijsKesselsARRK_0-1745305952881.png

 

 

0 Kudos
Reply

1,382 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I mass erased S32K144EVB-Q100, and the reset pin signal is exactly the same as yours.
But when I use the connect command of J-Link Command or Target->Connect of J-Flash, the reset pin will no longer reset periodically, and the program can be downloaded.

0 Kudos
Reply

1,375 Views
ThijsK
Contributor III

When I desolder the SBC and power the MCU directly with 5V, I do get the expected behavior you're also getting on the EVB:

ThijsKesselsARRK_0-1745411012217.bmp

So there is some interplay with the SBC, but what...

0 Kudos
Reply

1,271 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

I only support S32K and I am not familiar with FS23 products. 
But according to my experience, if FS23 does not enter debug mode, then you need to feed the watchdog. Since your S32K1 has not downloaded the program and cannot feed the watchdog, FS23 will generate a reset signal to reset the S32K1.
The circuit on the S32K3+FS23 board is designed to allow FS23 to enter debug mode (normal power supply but no need to feed the watchdog).
If it is in the design evaluation stage (the S32K1 program does not yet include FS23 configuration and feeding the watchdog), it is recommended to refer to the S32K3 board to design the debug mode circuit.

Note: This power-up procedure manages that FS23 SBC starts with a disabled watchdog:

https://www.nxp.com/document/guide/getting-started-with-the-s32k31xevb-q100-evaluation-board-for-gen...

Here is the schematic: S32K31XEVB-Q100 Evaluation Design Files 

Please follow Figure 15. Debug mode.png to let the FS23 enter debug mode.

0 Kudos
Reply

1,376 Views
ThijsK
Contributor III

When I "unlock Kinetis" in J-Link commander RESET is released for ±200ms:

ThijsKesselsARRK_0-1745410648050.bmp

When I "connect" in J-Link (S32K144, SWD, 4000kHz), J-Link seems happy:

J-Link>connect
Device "S32K144" selected.


Connecting to target via SWD
ConfigTargetSettings() start
ConfigTargetSettings() end - Took 11us
InitTarget() start
SWD selected. Executing JTAG -> SWD switching sequence.
InitTarget() end - Took 162ms
Found SW-DP with ID 0x2BA01477
DPIDR: 0x2BA01477
CoreSight SoC-400 or earlier
AP map detection skipped. Manually configured AP map found.
AP[0]: AHB-AP (IDR: Not set, ADDR: 0x00000000)
AP[0]: Core found
AP[0]: AHB-AP ROM base: 0xE00FF000
CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)
Found Cortex-M4 r0p1, Little endian.
FPUnit: 6 code (BP) slots and 2 literal slots
CoreSight components:
ROMTbl[0] @ E00FF000
[0][0]: E000E000 CID B105E00D PID 000BB00C SCS-M7
[0][1]: E0001000 CID B105E00D PID 003BB002 DWT
[0][2]: E0002000 CID B105E00D PID 002BB003 FPB
[0][3]: E0000000 CID B105E00D PID 003BB001 ITM
[0][4]: E0040000 CID B105900D PID 000BB9A1 TPIU
Memory zones:
Zone: "Default" Description: Default access mode
Cortex-M4 identified.

However, RESET is only released for 750ms

ThijsKesselsARRK_1-1745410894735.bmp

 

0 Kudos
Reply