S32K144 FLEXSPI/LPSPI CS pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 FLEXSPI/LPSPI CS pin

Jump to solution
2,259 Views
antoine_monmarc
Contributor V

Hello,

I'm using spi_pal demo from SDK S32DS_ARM_v2018.R1.

The master is configured to use FLEXIO SPI.

I have a question related to the CS pin. As you can see on the picture below, the CS is disabled between every bytes.

pastedImage_1.png

Is there a way to enable the CS pin as long as the master has data to transmit?

I looked into the FLEX SPI driver but I'm not familliar with it.

From Master side (running on another S32k148EVB board), it seems that the LPSPI IRQ is not triggered when the CS is enabled/disabled. I tryed to confirgure the interrupt on PTB0 using INT_SYS_EnableIRQ and INT_SYS_InstallHandler but it seems that it's never triggered.

Aslo the lpspi Callback is not triggered when the CS pin status change.

0 Kudos
Reply
1 Solution
2,007 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

This feature is not available in Flexio, but you can use it on LPSPI. Please switch to LPSPI and select continuous mode.

In this mode CS is assert for all frames which are configured in your sending function.

I don't get exactly what are you trying to do with with the next SPI. Why both of them are masters? 

If PTB0 is routed to Flexio you can't use it as GPIO.

Best regards,

Razvan

View solution in original post

0 Kudos
Reply
3 Replies
2,007 Views
antoine_monmarc
Contributor V

Hello,

Yes by changing the master from Flexio to LPSPI we were able to use the continuous mode.

thank you.

0 Kudos
Reply
2,008 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

This feature is not available in Flexio, but you can use it on LPSPI. Please switch to LPSPI and select continuous mode.

In this mode CS is assert for all frames which are configured in your sending function.

I don't get exactly what are you trying to do with with the next SPI. Why both of them are masters? 

If PTB0 is routed to Flexio you can't use it as GPIO.

Best regards,

Razvan

0 Kudos
Reply
2,007 Views
nxf47370
NXP Employee
NXP Employee

Hi, Razvan-nicolae,

I noticed the S32K1xx RM Chapter 52.5.3" For CPHA=1, the select can remain asserted for multiple transfers and the timer status flag can be used to indicate the end of the transfer."  Does it mean that it can enable the CS pin as long as the master has data to transmit? If not, what does it mean?

Thanks, BR,

Han

0 Kudos
Reply