S32K144 EVB board How to power with 5v usb adaptor not pc usb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 EVB board How to power with 5v usb adaptor not pc usb

338 Views
alice_thanks
Contributor III

with S32K144 EVB board i find it only connect with pc usb port the board can power up, when connect with 5v usb adaptor , the board can't power.

How to power board with 5v usb adaptor ?

0 Kudos
Reply
2 Replies

320 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

When connect with 5v usb adaptor, the MK20DX128VFM5 did not output high voltage at POWER_EN signal. So it disable 5v from USB connector.

POWER_EN VTRG_EN MIC2005.png


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

302 Views
alice_thanks
Contributor III

Ok, thanks @Robin_Shen 

another quesiton about i2c not work with freertos, could you help to check it 

please see attached code

also i have raise ticket before, but can't resolved it

https://community.nxp.com/t5/S32K/s32k144-FreeRTOS-I2C/m-p/1677024

 

0 Kudos
Reply