I'm working with the S32K144 evaluation board But I'm having some errors using UART in FreeRTOS I got source FreeRTOS_printf_SDKv0_8_6 and In S32DS ARM R1 compiled but fatal error: No such file or directory (ewl_misra_types.h and file_struc.h )
Hi,
seems you are pointing to example posted here EXAMPLE: S32k144 UART printf/scanf under FreeRTOS - S32DS
I have downloaded it and imported it to the S32 DS ARM 2018.R1. I see no issue with compiling, I got no errors.
ewl_misra_types.h and file_struc.h files should be located in below directories within DS installation
..\S32DS_ARM_v2018.R1\S32DS\arm_ewl2\EWL_C\include\
..\S32DS_ARM_v2018.R1\S32DS\arm32_ewl2\EWL_C\include\
check those directories and be sure one is listed in project's path
BR, Petr
Thank you for your answer
so I made it in consideration of your answer , It have mistakes for
importing of source file
I have concern about free RTOS with S32k144
but a little bit progressed,
I will ask more question
Thank you a lot
2019년 3월 26일 (화) 오전 9:30, jungtaek HEO <daxorcom2@gmail.com>님이 작성:
Hi thanks
It works
>
2019년 3월 20일 (수) 오전 1:16, PetrS <admin@community.nxp.com>님이 작성:
>>
>> * NXP Community
>> <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
>> Re: S32K144 EVB LPUART in FreeRTOS reply from Petr Stancik
>> <https://community.nxp.com/people/PetrS?et=watches.email.thread> in S32K -
>> View the full discussion
>> <https://community.nxp.com/message/1126850?commentID=1126850&et=watches.email.thread#comment-1126850>
>>
Hi thanks
It works
2019년 3월 20일 (수) 오전 1:16, PetrS <admin@community.nxp.com>님이 작성:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: S32K144 EVB LPUART in FreeRTOS reply from Petr Stancik
<https://community.nxp.com/people/PetrS?et=watches.email.thread> in S32K -
View the full discussion
<https://community.nxp.com/message/1126850?commentID=1126850&et=watches.email.thread#comment-1126850>