S32K144_EVB,FreeMASTER

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144_EVB,FreeMASTER

942 Views
taotao
Contributor I
按您说的将S32K144_EVB_JumpStart_Firmware.srec复制到开发板的驱动盘后,在FreeMASTER上connection wizard 按use direct connection to on-board US以波特率115200连接,,按操作接好设备,连接依然报错,报错为无法从链接打开项目文件'http://www.nxp.com/assets/downloads/data/en/application-software/s32K144EVB_OOBE.pmpx"
0 Kudos
1 Reply

931 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@taotao

         这个版本的Freemaster软件是老版本S32 Design Studio for ARM v2.0上的,用新版本需要自己移植过来,如果你不想移植的话,可以直接将旧版本的srec文件或者elf文件烧写到开发板上,。我用S32K142EVB示范.

1.单独烧写srec或者elf.(因为我用的是J-LINK,你如果用PE工具就选第一个),选择完以后可以在Debugger栏看看烧写器的配置,最后点击Flash就可烧写进去。

Senlent_0-1634539111867.png

 

2.上面这一步就是将旧版本的工程烧写到开发板中,现在这一步就是用Freemaster打开工程,建立链接。

a.打开Freemaster软件,File->Open Project,选择S32K142_EVB_JumpStart.pmpx.(你的是S32K144,操作原理一样)。

b.Tool->connect.....和你的提问中的回答一样操作,一直next就成功了。下图是我成功操作后的截图,工作正常。

Senlent_1-1634539555225.png

 

3.看你的报错是不是没有选择Open->Project,选择S32K142_EVB_JumpStart_PC文件夹中的.pmpx文件,亦或者是不是没有烧写好程序,总结就这两个步骤。

 

BR!

     Jim,

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos