S32K144 Debug Breakpoint Qustions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Debug Breakpoint Qustions

1,759 Views
Raphael2
Contributor III

Hi,

I got some questions about the breakpoints in debug mode. Below is a simple program to explain.

Putting breakpoints before the first 3 lines in main just works as expected, but aren't declarations like  counter, and counter_limit able to stop the program? Is there a reason?

I tried putting a breakpoint before the LED toggle point PTD->PTOR = 1<<0; but it just gets ignored..?

And if I put it next line when counter is set to 0 again the program stops at this point every single cycle of the for loop (even if the if-request isn't true), and that confuses me most..

 

I hope someone can enlighten me

 

Best regards

Raphael

 

The Code:

 

#include "sdk_project_config.h"
#include "s32K144.h"

volatile int exit_code = 0;

int main(void)
{

PCC->PCCn[PCC_PORTD_INDEX] = PCC_PCCn_CGC_MASK; //enabling clock for PORT D
PORTD->PCR[0] = PORT_PCR_MUX(1); //set pin as GPIO
PTD->PDDR = 1<<0; // pin 0 is configured as output
int counter = 0;
int counter_limit = 100000;


for(;;)
{
counter++;

if(counter > counter_limit)
{
PTD->PTOR = 1<<0;
counter = 0;
}

if(exit_code != 0)
{

break;
}
}
return exit_code;
}

0 Kudos
Reply
1 Reply

1,748 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Raphael2

              This may be caused by the different locations of variables in memory, and the debugger cannot access this storage space.

The shaded part on the left is where breakpoints can be placed.(I use KEIL to port you code.)

Here is you code,

Senlent_0-1627957493747.png

Turn it into a global variable

Senlent_1-1627957638630.png

That's all I know, and I hope this answer is useful to you.

BR!

Jim.

 

 

0 Kudos
Reply