S32K144 CAN configuration with range of IDs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 CAN configuration with range of IDs

4,446 Views
AnilKumar409
Contributor III

Hi,

I configured CAN communication with MB0 as Tx buffer with ID 511 and MB4 as Rx buffer with ID 555.

Now I need to use range of IDs from 100 to 108 for data reception. Can you help me to make arrangements in the S32K DS code.

0 Kudos
Reply
7 Replies

4,388 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@AnilKumar409

modified base on the demo of S32K144_Project_FlexCan

MB1 used for receiving messages which id range of 0x100~0x107,

(in this case,0x108 need to be allocated a MB for it separately)

void FLEXCAN0_init(void)
{
#define MSG_BUF_SIZE  4		/* Msg Buffer Size. (CAN 2.0AB: 2 hdr +  2 data= 4 words) */
  uint32_t   i=0;

  PCC->PCCn[PCC_FlexCAN0_INDEX] |= PCC_PCCn_CGC_MASK; /* CGC=1: enable clock to FlexCAN0 */

  CAN0->MCR |= CAN_MCR_MDIS_MASK;         /* MDIS=1: Disable module before selecting clock 	*/
  CAN0->CTRL1 &= ~CAN_CTRL1_CLKSRC_MASK;  /* CLKsrc=0: Clock Source = SOSCDIV2				*/
  CAN0->MCR &= ~CAN_MCR_MDIS_MASK;        /* MDIS=0; Enable module config. (Sets FRZ, HALT)	*/

  while (!((CAN0->MCR & CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT))  {}
	/*!
	 * Good practice:
	 * ===================================================
	 * wait for FRZACK=1 on freeze mode entry/exit
	 */

  //Enable the individual filtering per MB and reception queue features
  CAN0->MCR |= CAN_MCR_IRMQ(1);

  //Disable Rx FIFO
  CAN0->CTRL2 = 0 | CAN_CTRL2_EACEN(0);


  CAN0->CTRL1 = 0
      #if defined(S32K11x_SERIES)
      |CAN_CTRL1_PRESDIV(4)   /* PRESDIV=4: Sclock=PEclock/(PRESDIV+1) = 40MHz/5 = 8MHz    */
      #endif
      |CAN_CTRL1_PSEG2(3)	    /* Configure for 500 KHz bit time 								*/
		  |CAN_CTRL1_PSEG1(3) 		/* Time quanta freq = 16 time quanta x 500 KHz bit time= 8MHz 	*/
		  |CAN_CTRL1_PROPSEG(6)		/* PRESDIV+1 = Fclksrc/Ftq = 8 MHz/8 MHz = 1 					*/
		  |CAN_CTRL1_RJW(3)			/*    so PRESDIV = 0 											*/
		  |CAN_CTRL1_SMP(1); 		/* PSEG2 = Phase_Seg2 - 1 = 4 - 1 = 3 							*/
								            /* PSEG1 = PSEG2 = 3 											*/
									/* PROPSEG= Prop_Seg - 1 = 7 - 1 = 6 							*/
									/* RJW: since Phase_Seg2 >=4, RJW+1=4 so RJW=3. 				*/
									/* SMP = 1: use 3 bits per CAN sample 							*/
									/* CLKsrc=0 (unchanged): Fcanclk= Fosc= 8 MHz 					*/

  for(i=0; i<128; i++ )
  {   					/* CAN0: clear 32 msg bufs x 4 words/msg buf = 128 words */
    CAN0->RAMn[i] = 0;  /* Clear msg buf word */
  }
  for(i=0; i<16; i++ )
  {          						/* In FRZ mode, init CAN0 16 msg buf filters */
    CAN0->RXIMR[i] = 0xFFFFFFFF;  	/* Check all ID bits for incoming messages */
  }
//CAN0->RXMGMASK = 0x1FFFFFFF;  				/* Global acceptance mask: check all ID bits 	*/
  CAN0->RAMn[ 4*MSG_BUF_SIZE + 0] = 0x04000000; /* Msg Buf 4, word 0: Enable for reception 	*/
                                                /* EDL,BRS,ESI=0: CANFD not used 				*/
                                               /* CODE=4: MB set to RX inactive 				*/
                                                /* IDE=0: Standard ID 							*/
                                                /* SRR, RTR, TIME STAMP = 0: not applicable 	*/

  /* Node B to receive msg with std ID 0x555 	*/
  CAN0->RAMn[ 4*MSG_BUF_SIZE + 1] = 0x555 << 18; /* Msg Buf 4, word 1: Standard ID = 0x555 		*/



  CAN0->RAMn[ 1*MSG_BUF_SIZE + 0] = 0x04000000;
  CAN0->RAMn[ 1*MSG_BUF_SIZE + 1] = 0x100 << 18;//Standard ID = 0x100

  //receive range of standard IDs of 0x100~0x107
  CAN0->RXIMR[1] = 0x1FE3FFFF;


  CAN0->MCR |=((0x0000001F) | (1 << 17));//SRXDIS = 1,MAXMB = 32

  CAN0->MCR &=~CAN_MCR_HALT_MASK;	//Netate HALT bit


  while ((CAN0->MCR && CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT)  {}
  /* Good practice: wait for FRZACK to clear (not in freeze mode) */

  while ((CAN0->MCR && CAN_MCR_NOTRDY_MASK) >> CAN_MCR_NOTRDY_SHIFT)  {}
  /* Good practice: wait for NOTRDY to clear (module ready) */
}

 

main.c

When a frame with ID 0x100 to 0x107 is received, the led light will flash

	  for (;;)
	  {                        			/* Loop: if a msg is received, transmit a msg */
		if ((CAN0->IFLAG1 >> 4) & 1) {  /* If CAN 0 MB 4 flag is set (received msg), read MB4 */
		  FLEXCAN0_receive_msg ();      /* Read message */
		  rx_msg_count++;               /* Increment receive msg counter */

		  if (rx_msg_count == 1000) {   /* If 1000 messages have been received, */
			PTD->PTOR |= 1<<16;         /*   toggle output port D16 (Green LED) */
			rx_msg_count = 0;           /*   and reset message counter */
		  }
		  FLEXCAN0_transmit_msg ();     /* Transmit message using MB0 */
		};

		if((CAN0->IFLAG1 >> 1) & 1)
		{
			CAN0->IFLAG1 = 0x00000002;       /* Clear CAN 0 MB 1 flag without clearing others*/
			PTD->PTOR |= 1<<16;
		}

	  }

 

BR!

 

 

0 Kudos
Reply

4,380 Views
AnilKumar409
Contributor III

Hi @Senlent ,

Thank you for your support...

I have gone through your demo code. Can you make brief about this line,

//receive range of standard IDs of 0x100~0x107

CAN0->RXIMR[1] = 0x1FE3FFFF;

I was not able to understand how it got defined.

0 Kudos
Reply

3,922 Views
aug
Contributor I

fhdyhdF'h

0 Kudos
Reply

4,372 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@AnilKumar409

Senlent_1-1665648876062.png

 

 

0 Kudos
Reply

4,361 Views
AnilKumar409
Contributor III

Thank you @Senlent 

0 Kudos
Reply

4,426 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@AnilKumar409

There is a  demo in our community , you can refer to

https://community.nxp.com/t5/S32K-Knowledge-Base/S32K1xx-FlexCAN-Mask-Setting-Demo/ta-p/1519753 

If you have any questions about this demo, please let me know!

BR!

0 Kudos
Reply

4,422 Views
AnilKumar409
Contributor III

Can I get a reference code or guidelines written by experts instead of Processor Expert generated. It difficult to me for understanding this code as I'm a beginner. How to make arrangement of registers like RXIMR and RXMGMASK. Find below CAN initialization

void CAN0_init(void){
#define MSG_BUF_SIZE 4
uint32_t i = 0;
PCC->PCCn[PCC_FlexCAN0_INDEX] |= PCC_PCCn_CGC_MASK;
CAN0->MCR |= CAN_MCR_MDIS_MASK;
CAN0->CTRL1 &= ~(CAN_CTRL1_CLKSRC_MASK);
CAN0->MCR &= ~CAN_MCR_MDIS_MASK;
while(!((CAN0->MCR & CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT));
CAN0->CTRL1 = 0x00DB0006;
for(i=0;i<128;i++){
CAN0->RAMn[i] = 0;
}
for(i=0;i<16;i++){
CAN0->RXIMR[i]=0xFFFFFFFF;
}
CAN0->RXMGMASK = 0x1FFFFFFF;
CAN0->RAMn[4*MSG_BUF_SIZE + 0] = 0x04000000;
CAN0->RAMn[4*MSG_BUF_SIZE + 1] = 0x04000000; /* ID 0100 */
CAN0->IMASK1 = 0x00000010;
CAN0->MCR = 0x0000001F;
while((CAN0->MCR && CAN_MCR_FRZACK_MASK) >> CAN_MCR_FRZACK_SHIFT);
while((CAN0->MCR && CAN_MCR_NOTRDY_MASK) >> CAN_MCR_NOTRDY_SHIFT);
}

0 Kudos
Reply