S32K144 Board is not found in S32 Design Studio

cancel
Showing results for 
Search instead for 
Did you mean: 

S32K144 Board is not found in S32 Design Studio

Jump to solution
209 Views
Raphael2
Contributor III

Hi,

 

I imported an example project, build it without errors and want to flash it now.

But :

Praemas_0-1625663854878.png

The Controller cannot be found by the program.

But the board is connected in the device manager.

What am I missing?

 

Best regards

0 Kudos
1 Solution
207 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Raphael2,

How did you connect the board to your PC? Did you use the USB Multilink device from P&E Micro and connect it to the PC via USB and the board via JTAG? That is the option shown in the image provided.

If you are instead connecting directly to the eval board, using only a USB cable, then you will want to select the option 'OpenSDA Embedded Debug - USB Port'.

Best Regards,

Mike

View solution in original post

0 Kudos
2 Replies
179 Views
Raphael2
Contributor III

Hello @mikedoidge,

thank you,

I guess I missed to change in debug configurations.

I tried an example project and flashing the board works.

Best Regards

0 Kudos
208 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Raphael2,

How did you connect the board to your PC? Did you use the USB Multilink device from P&E Micro and connect it to the PC via USB and the board via JTAG? That is the option shown in the image provided.

If you are instead connecting directly to the eval board, using only a USB cable, then you will want to select the option 'OpenSDA Embedded Debug - USB Port'.

Best Regards,

Mike

View solution in original post

0 Kudos