S32K144 ADC channel collet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K144 ADC channel collet

462件の閲覧回数
547416104
Contributor III

Hello EveryOne,

I just config AD00 and AD01, AD112,AD113 channels to do ADC collect, but I find the AD00 channel ADC value  is affected by AD01, AD112 is affected by AD113, whether I config is wrong, thanks

547416104_0-1669643329770.png

547416104_1-1669643343376.png547416104_2-1669643347056.png

547416104_3-1669643353607.png

547416104_4-1669643392290.png547416104_5-1669643408778.png

 

547416104_6-1669643426249.png547416104_7-1669643439047.png

 

0 件の賞賛
返信
1 返信

455件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @547416104 

The S32K1's ADC has three main sub-blocks:

  • capacitive DAC
  • comparator
  • SAR

DAC is the most susceptible to the variations it can cause because it is designed with binary weighted capacitor arrays.

At the moment when you are using several channels of an ADC, the capacitors cannot be fully discharged when another measurement is already being made. I suggest you to set a delay between measurements to let the capacitors discharge.
Also, take a look to this application note and community post, it will be useful for you.

S32K1xx ADC guidelines, spec and configuration 

16-bit SAR ADC calibration 

 

B.R.

VaneB

0 件の賞賛
返信