S32K142 Download APP on PFlash, unsuccessful.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K142 Download APP on PFlash, unsuccessful.

1,042 次查看
yanren
Contributor I

Flash DRV Program () is used to download the corresponding data. When the -128 byte number of data is swiped, only 24 bytes of data are saved in the memory of PFlash. After that, the Program is stuck. When entering the debugging state to view the PFLASH memory, the data that was swiped before was not saved.

1626229649040.jpg

0 项奖励
回复
1 回复

1,027 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

can I see input parameters for FLASH_DRV_Program() function when the problem appears? Does it work if you disable interrupts before calling of this function?

Regards,

Lukas

0 项奖励
回复