S32K142 Download APP on PFlash, unsuccessful.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K142 Download APP on PFlash, unsuccessful.

1,040件の閲覧回数
yanren
Contributor I

Flash DRV Program () is used to download the corresponding data. When the -128 byte number of data is swiped, only 24 bytes of data are saved in the memory of PFlash. After that, the Program is stuck. When entering the debugging state to view the PFLASH memory, the data that was swiped before was not saved.

1626229649040.jpg

0 件の賞賛
返信
1 返信

1,025件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

can I see input parameters for FLASH_DRV_Program() function when the problem appears? Does it work if you disable interrupts before calling of this function?

Regards,

Lukas

0 件の賞賛
返信