S32K142 Download APP on PFlash, unsuccessful.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K142 Download APP on PFlash, unsuccessful.

1,043 Views
yanren
Contributor I

Flash DRV Program () is used to download the corresponding data. When the -128 byte number of data is swiped, only 24 bytes of data are saved in the memory of PFlash. After that, the Program is stuck. When entering the debugging state to view the PFLASH memory, the data that was swiped before was not saved.

1626229649040.jpg

0 Kudos
Reply
1 Reply

1,028 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

can I see input parameters for FLASH_DRV_Program() function when the problem appears? Does it work if you disable interrupts before calling of this function?

Regards,

Lukas

0 Kudos
Reply