S32K14 IIC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K14 IIC

2,809 Views
gravity_one
Contributor III

hello,

use LPIIC,

I want to read IMU(BMI160) device info on IIC bus,device addr is 0x68,The register address is 0x0,

how to do ?

thanks

0 Kudos
17 Replies

2,524 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

You may download the SDK for the S32K14x. Here you will find many examples using the I2C module. You can use these as a reference to connect your device via I2C.

To download the SDK please use this link.

Best Regards,

Sabina

0 Kudos

2,524 Views
gravity_one
Contributor III

hello,

no use freeRTos,

sta=LPI2C_DRV_MasterSendDataBlocking(INST_LPI2C1, buffer, 1, true, 0xFFFFFFFF);
sta=LPI2C_DRV_MasterReceiveDataBlocking(INST_LPI2C1, buffer, 1, true, 0xFFFFFFFF);

can read  device ID,

but add freeRTos,

cannot read ID,return sta is busy.

0 Kudos

2,524 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Do you try to send date outside of you tasks? If yes, please  modify  your code to do not call any function which can trigger interrupts before vTaskStartScheduler().

Best regards,

Razvan

0 Kudos

2,524 Views
gravity_one
Contributor III

hello,

i konw,

i try to it before vTaskStartScheduler().but it failure,

Best regards,

Grayli

0 Kudos

2,524 Views
razva_tilimpea
NXP Employee
NXP Employee

Can you send a snippet of code to understand how do you use I2C and freeRtos?

0 Kudos

2,524 Views
gravity_one
Contributor III

hello,

sorry,i try to it before vTaskStartScheduler().it ok today.

but , i want to read after vTaskStartScheduler();

how to do?  into  taskENTER_CRITICAL(); it failure,

Best regards,

Grayli

0 Kudos

2,524 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

I don't know how your application works, but I would try to move that I2C code inside your task.

If you need that I2C call for one time initialization purpose you can create a task which is run only one time and after that you can remove it.

Probably your problem is similar to what is discussed here: What is normal method for running initialization code in FreerTOS? - FreeRTOS .

Best regards,

Razvan

0 Kudos

2,524 Views
gravity_one
Contributor III

thanks,

Are there any examples of GPIO emulating the IIC bus?

I used PTA-0/1 to simulate IIC  on s32k146-64pin

0 Kudos

2,524 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

We do not have this type of driver for S32K1xx parts because there a lot of peripherals which can be used for I2C ( LPI2C and FlexIO). 

I don't recommend to use bit-banging because it will rise many issues.

Best regards,

Razvan

0 Kudos

2,524 Views
gravity_one
Contributor III

hello,

Did you get my mail?

Best regards,

Grayli

0 Kudos

2,523 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

I didn't get anything from your side. If is possible please share your project here.

Best regards,

Razvan

0 Kudos

2,524 Views
gravity_one
Contributor III

发件人: bounces+210748-7d9b-grayli.wang=cdskysoft.com@jiveon.jivesoftware.com 代表 razva_tilimpea

发送时间: 2020年1月13日 16:49

收件人: WANG LI

主题: Re: - Re: S32K14 IIC

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: S32K14 IIC

reply from Razvan-nicolae Tilimpea <https://community.nxp.com/people/razva_tilimpea?et=watches.email.thread> in S32K - View the full discussion <https://community.nxp.com/message/1254389?commentID=1254389&et=watches.email.thread#comment-1254389>

0 Kudos

2,524 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

The main problem with this application is that state structure (lpi2c1MasterState) is overwrite by some internal calls of the FreeRTOS. I don't understand exactly why this is happening (probably FreeRTOS suppose that you don't need to use again variables from main stack), but the easy fix is to move this state structure outside of stack by declaring it as global. In this way you won't have any overlap between main stack and other tasks tasks.

Also, please add INT_SYS_SetPriority(LPI2C0_Master_IRQn, 2); before starting scheduler to match maximum system call interrupt priority restriction.

Best regards,

Razvan

0 Kudos

2,524 Views
gravity_one
Contributor III

hello,

lpi2c_master_state_t *master;   Is it defined as a global variable?

but it is failure.

Have you tested your method?

Please specify the specific operation steps, or you know to help modify the code!

The way you said above is too abstract for me to understand.

lpi2c_master_state_t *master;

status_t LPI2C_DRV_MasterSendDataBlocking(uint32_t instance,const uint8_t * txBuff,uint32_t txSize,bool sendStop,uint32_t timeout)
{

DEV_ASSERT(instance < LPI2C_INSTANCE_COUNT);
DEV_ASSERT(txBuff != NULL);
DEV_ASSERT(txSize > 0U);

master = g_lpi2cMasterStatePtr[instance];
DEV_ASSERT(master != NULL);

/* Check if driver is busy */
if(!master->i2cIdle)
{
return STATUS_BUSY;
}

/* mark transfer as blocking */
master->blocking = true;

/* Dummy wait to ensure the semaphore is 0, no need to check result */
(void)OSIF_SemaWait(&(master->idleSemaphore), 0);

(void)LPI2C_DRV_MasterSendData(instance, txBuff, txSize, sendStop);

/* Wait for transfer to end */
return LPI2C_DRV_MasterWaitTransferEnd(instance, timeout);
}

thanks

0 Kudos

2,524 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi,

Check attached project.

LPI2C initialization must be inside taks because inside of the driver some OS services are used.

I wasn't able to fully test it because I don't have your I2C slave devices.

Razvan

0 Kudos

2,524 Views
gravity_one
Contributor III

Don't know how to add files

0 Kudos

2,524 Views
gravity_one
Contributor III

hello,
There is a real problem with your SDK. I created a new RTOS today, and only two tasks are running, that is, 1S reads the IIC once, both of which are wrong.

Send the code to your mailbox.

please review.

thanks

0 Kudos