S32K118EVB

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K118EVB

1,799件の閲覧回数
bhanu_nbkristee
Contributor I

hallo,

I am using S32K118EVB MCU. I connected usb to pc and other port to microcontroller. Power is not supplying to it. By default jumper J107 are in 1-2 position.But I have to configure 2-3 position. How to install J107 in 2-3 position?

Kind regards,

Bhanu

タグ(3)
0 件の賞賛
返信
1 返信

1,714件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Bhanu,

You are correct, if you want to power your board through an USB cable you need to connnect J107 to 2-3. To do this you need to put the jumper as shown in the below image.

pastedImage_1.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------