Hi, 我在使用S32K118中遇到了一个问题,就是在Bootloader时候,TX会出现下拉情况。想知道FlexCan在未初始化的时候。CAN的TX和RX引脚的状态是如何的?这个在S32芯片手册未看到相关定义。以及CAN初始化了,但是未对引脚进行配置。这个时候TX和RX的状态又是如何?
Hi,
once CAN function is selected within respective port PCR register, then TXD becomes high to serve recessive level and RXD is input, which is driven by connected transceiver.
BR, Petr