Hi,
I want to implement bootloader for s32k118 EVB. If I am flashing the code with debugger from any start address, after jumping to that address my application is running properly. But if I am writing same application hex file using FTFC then after jumping it reset the controller.
I have tested Flash read, write and erase. It is working fine. And I have disabled watchdog also. what is the issue I am not able to find?
Please help with the required information.
Thanks and regards,
Ravi Ranjan Kumar.
Can anybody help me with required information..?
Hello Ravi Ranjan Kumar,
Sorry for the late response. I recommend you checking the application note AN12218 (link). This application note explains how to make a bootloader for the S32K. You can download the software from the following link.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------