S32K118外接8M晶振,CAN外设采用外部8M晶振时钟,CAN的波特率在500K,采样点配置不到在75~80%,芯片可以刚好配置在75%和81.25%,配置在75%过不了车厂实验,能否配置到75~80%之间呢?
Solved! Go to Solution.
试了好多配置,没找到精确的500K&80%采样率的,75%倒是可以。
还是我上面说的,500K的速率最佳采样率大约在80%~87.5%最佳了,500K以上的速率大约在75%~80%
你的采样点为87%,能否调到75~80%之间?
采样率应该和你通讯速率有关系,500K的话大约至少在80%最佳,可以配置为87.5%,为什么不用这个采样率呢?
这个配置的采样率大约在80%左右,我这边没有测试的工具,没法验证这个配置能不能正常工作,需要你们自己测试一下。
试了好多配置,没找到精确的500K&80%采样率的,75%倒是可以。
还是我上面说的,500K的速率最佳采样率大约在80%~87.5%最佳了,500K以上的速率大约在75%~80%