S32K116 VLPS mode wake-up on arrival of a CAN message

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K116 VLPS mode wake-up on arrival of a CAN message

Jump to solution
401 Views
javher4127
Contributor I

Hello.

I would like to know if it is possible with the S32K116 microcontroller to wake up from VLPS power mode with the arrival of CAN messages.

Thanks.

0 Kudos
Reply
1 Solution
383 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @javher4127,

For S32K1 devices, self-wakeup from CAN module is not supported in VLPS mode. You can see that CAN module is OFF in Table 39-4. (Module operation in available power modes) from S32K-RM.

PNET features is used to wake up from STOP1/STOP2 modes in those instances where PNET is included, but this does not apply for VLPS mode. As a workaround, you can use any other pin (or even the same CAN_RX pin changing PORT configuration) to generate an interrupt when MCU is on VLPS mode. This can wake the CPU and then restore activity on CAN module.

Best regards,
Julián

View solution in original post

0 Kudos
Reply
3 Replies
384 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @javher4127,

For S32K1 devices, self-wakeup from CAN module is not supported in VLPS mode. You can see that CAN module is OFF in Table 39-4. (Module operation in available power modes) from S32K-RM.

PNET features is used to wake up from STOP1/STOP2 modes in those instances where PNET is included, but this does not apply for VLPS mode. As a workaround, you can use any other pin (or even the same CAN_RX pin changing PORT configuration) to generate an interrupt when MCU is on VLPS mode. This can wake the CPU and then restore activity on CAN module.

Best regards,
Julián

0 Kudos
Reply
275 Views
javher4127
Contributor I

PNET feature is CAN FD compatible?

Thanks.

0 Kudos
Reply
268 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @javher4127,

No, wakeup functionality is not available for messages in CAN FD format. When in Pretended Networking mode, CAN FD format messages are ignored.

0 Kudos
Reply