Hi, i´m trying the demo project lin_slave_s32k116 in a S32K116EVB2Q048 and the board doesn´t receive nor transmit any message. I´ve used an oscilloscope to check if the signal was corrrectly arriving to the LIN-associated pin, and that´s ok.
During the first attempts, as it comes configured by default in the demo, the LIN Rx/Tx pin were PTC6/PTC7. The communications doesn´t work, so that i changed these pins to PTC8/PTC9 and communications are not working yet.
I guess the problem may be in the transceiver wake-up process, but i don´t know. The instructions to wake-up the transceiver are the following:
````
/* Set LIN transceiver sleep pin direction */
PINS_DRV_SetPinsDirection(PTA, (0x1u << 7UL));
/* Wake up LIN transceiver */
PINS_DRV_SetPins(PTA, (0x1u << 7UL));
```
Thanks for your help, regards.