S32K116 ERM EAR0 has an fixed offset

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32K116 ERM EAR0 has an fixed offset

ソリューションへジャンプ
1,506件の閲覧回数
Helloyt
Contributor III

Hi,

    I tried to test the feedback of ERM when i read different area of SRAM with signal bit ECC error injected, but wen i test the address of SRAM_U  in S32K116 with SDK3.0.0 ,I found that it always has an fixed offset 0x3C(if the read SRAM_U address greater than 0x20003800 - 0x3C ,the EAR0 will always be 0x200037FC)

    p.s. optimization level is -O0

    followint are the debug pics: 

  • pic1

Helloyt_0-1689902923015.png

  • pic2

Helloyt_1-1689902976190.png

  • pic3

Helloyt_3-1689903625499.png

 

address i tried to read:

#define MEM_TEST_ADDRESS1 (uint32_t *)0x20000000U
#define MEM_TEST_ADDRESS2 (uint32_t *)0x20003000U
#define MEM_TEST_ADDRESS3 (uint32_t *)0x200037E0U

in pic1 and pic2 , you can see than when i read 0x20000000 ,with EAR0 0x2000003C feedback

when i read 0x20003000 with EAR0 0x200000C0 feedback

and in pic3 ,when i tried to read 0x200037E0 with 0x200037FC feedback

  • pic4

Helloyt_4-1689903945123.png

but,inexplicably,sometimes it could feedback the right address ,as you see in pic4,with no config changed 

I realized that if i set breakpoint before i read specific address and use signal step to debug,it will generate a 0x3c offset although all disassmbly access are right(i need to check disassembly code),but when i set breakpoint after the read access ,the offset seems will not generate anymore.

so what would response to the error?

 

 

0 件の賞賛
返信
1 解決策
1,442件の閲覧回数
Helloyt
Contributor III

Hi,@Robin_Shen

Thanks for your answer, my IDE is S32DS 2018 wih SDK3.0.0 ,but I supposed that the main difference is that my debugger is Jlink.

the first time I try to debug step by step, it has an fixed offset but after a SW reset by debugger, the offset not occurred any more.

by the way, I found that if I debug step by step meanwhile read the data in memory , the offset also changed, So it seems the best solution for any debug device is to run without pause

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,477件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I debug it with on board OpenSDA, set only one breakpoint before read specific address. It did not generate a 0x3c offset.

read MEM_TEST_ADDRESS1.pngread MEM_TEST_ADDRESS3.pngread MEM_TEST_ADDRESS2.png


Best Regards,
Robin

1,443件の閲覧回数
Helloyt
Contributor III

Hi,@Robin_Shen

Thanks for your answer, my IDE is S32DS 2018 wih SDK3.0.0 ,but I supposed that the main difference is that my debugger is Jlink.

the first time I try to debug step by step, it has an fixed offset but after a SW reset by debugger, the offset not occurred any more.

by the way, I found that if I debug step by step meanwhile read the data in memory , the offset also changed, So it seems the best solution for any debug device is to run without pause

0 件の賞賛
返信