S32K116, Cannot detect the board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K116, Cannot detect the board

跳至解决方案
630 次查看
tole
Contributor I

Hello.

I tried Debugging several times on S32DS ARM 2.2 application. 

And could not detect the board. 

On window - Device Manager, I can find the Port name with OpenSDA. But not allow to use it.

tole_0-1742046185748.png

tole_1-1742046466922.png

What shall I have to do??

 

0 项奖励
回复
1 解答
594 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I don't have DEVKIT-MOTORGD board, so just try to program MCSPTE1AK116_PMSM_FOC_2Sh project to S32K116EVB2Q048. I didn't encounter this problem, here is my configuration:

Debug Configuration MCSPTE1AK116_PMSM_FOC_2Sh.pngS32 Design Studio for ARM Installation Details MCSPTE1AK116_PMSM_FOC_2Sh.png

Did the LED D3 light? I want to make sure that the S32K116 is powered.

It is also recommended to refer to the suggestions in https://community.nxp.com/t5/S32K/Error-Launching-code-in-S32DS-v3-4/td-p/1901722.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
595 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

I don't have DEVKIT-MOTORGD board, so just try to program MCSPTE1AK116_PMSM_FOC_2Sh project to S32K116EVB2Q048. I didn't encounter this problem, here is my configuration:

Debug Configuration MCSPTE1AK116_PMSM_FOC_2Sh.pngS32 Design Studio for ARM Installation Details MCSPTE1AK116_PMSM_FOC_2Sh.png

Did the LED D3 light? I want to make sure that the S32K116 is powered.

It is also recommended to refer to the suggestions in https://community.nxp.com/t5/S32K/Error-Launching-code-in-S32DS-v3-4/td-p/1901722.

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复