S32K1 UART voltage levels

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K1 UART voltage levels

跳至解决方案
2,173 次查看
Vishnu3
Contributor III

Hi all,

I am using a BLE module operating at 3.3 volt UART, connected to LPUART of S32K1. Does the S32K1 support 3.3V at for its LPUART Rx and Tx? The Tx from LPUART to BLE module is working (with some hiccups) but the Rx at LPUART from BLE module is not working, I was thinking maybe the voltage levels could be an issue.

 

Best,

 

Vishnu

0 项奖励
回复
1 解答
2,131 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Vishnu3

Yes, I think this may be the cause of your level. You can use an oscilloscope to check it.

As i said before, S32K1 can work on 3.3V or 5V and the pin outputs voltage level depends on your S32K1 power supply voltage.

 

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,149 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Vishu3

you need to check the power supply of S32K1 which can work on 3.3V and 5V.

if 5V is used as power supply, then you may need some voltage levels converter.

0 项奖励
回复
2,137 次查看
Vishnu3
Contributor III

Hi Senlent,

 

Thanks for the reply. I checked my UART voltage level and it is at 5 V. Like I said, the data from S32K1 device to my target device (operating at 3.3V) is working. But the reverse path is not. Do you think it is because of the difference in voltage? 

 

At what voltage does NXP S32K144 register a logic high? What's the threshold? 

0 项奖励
回复
2,132 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Vishnu3

Yes, I think this may be the cause of your level. You can use an oscilloscope to check it.

As i said before, S32K1 can work on 3.3V or 5V and the pin outputs voltage level depends on your S32K1 power supply voltage.

 

0 项奖励
回复